README.TXT Drive composer entry 1.0.4.0 ========== 12.07.2012 ================================================================ *** BEFORE YOU START THE PROGRAM, PLEASE READ THIS CAREFULLY *** ================================================================ This file has been divided into the following sections for easy reference: 1. OVERVIEW 2. SAFETY INSTRUCTIONS 3. PREREQUIREMENTS 4. INSTALLATION 5. GETTING HELP 6. LIMITATIONS/CHANGES 1. OVERVIEW ---------------- Drive composer is a startup and maintenance PC tool for ABB's common architecture drive series such as ACS880, 580 etc. It is available with two versions entry and pro. Drive composer pro includes all entry features and much more such as data loggers, control diagrams, safety configuration and macro script. Drive composer pro will be available through ABB sales channels. Drive composer entry is available from ABB Web (www.abb.com/drives and select PC Tools) Drive composer entry/pro are designed to run under the Windows XP, Windows Vista and Windows 7 operating systems (32 and 64 bit operating systems). The key functions of Drive composer entry are the following: • Connect point-to-point to one drive using Assistant control panel's USB port • Show the actual status of the connected drive • View, edit and search the drive parameters • Show modified drive parameters (Not at default) • Save parameters from drive to PC and download parameters from PC to drive • Monitor drive signals graphically and numerically (Limited functionality) • Control a drive • Use of workspace and customized parameter windows 2. SAFETY INSTRUCTIONS ---------------- Follow these instructions when using the Drive composer entry PC tool. WARNING: Ignoring the following instructions can cause physical injury or death, or damage to the equipment. • When using the control panel of Drive composer entry, you can be far a way from the actual motor. Make sure that starting and stopping the drive and switching between LOC(local) and REM(remote) can be done safely. 3. PREREQUIREMENTS ---------------- • .NET 3.5 SP1 has to be installed on PC (included in Windows 7) with other operating system you can download and install from Microsoft's web page (http://www.microsoft.com/downloads/en/details.aspx?FamilyID=ab99342f-5d1a-413d-8319-81da479ab0d7) • Correctly installed drivers to PC for Assistant control panel are needed. Instructions how to do it can be found from Drive composer user's manual. • USB A/MINI B USB cable (max 3 m) is needed for connection • Free USB port on PC 4. INSTALLATION ---------------- Remove previous version of Drive composer entry from your PC. Unzip installation program that was downloaded from ABB Web to your PC. Double click Installation program setup.exe and follow the instructions for the installation. IF you have installed Assistant control panel drivers with previous version of Drive composer entry you can ignore installation of those drivers. 5. GETTING HELP ---------------- If you want help with Drive composer it is available from the following sources: - Please read the User Manual, found from installation folder of Drive composer entry or from Www.abb.com/drives select PC Tools). - Document about known problems is found from from Www.abb.com/drives select PC Tools). - Secondly please contact the local PC support persons. - Contact local ABB for more help. Please provide them with information like Windows operating system version, error message code etc. - A local ABB Sales office is also able to fetch information from ABB Library (http://inside.abb.com/Library). - If Drive composer crashes with " Send to ABB notice box" please send that information to ABB. 6. LIMITATIONS/CHANGES ---------------- 6.1 Entry version works only point-to-point connection to drive. 6.2 Firmware manual link working for parameters (right click on parameter andd select parameter help) 6.3 Older version saved monitor files not working with this version, changes made in monitored data file system because Drive composer pro is already released for sales. New extension of Drive composer monitor files for entry is (*.dcemon) Thank you for reading me!