README.TXT DriveStudio 1.5 SP ========== IMPORTANT: This Service Pack installs DriveStudio version 1.6. You can use this Service Pack ONLY IF you have DriveStudio version 1.5 in your computer. DO NOT uninstall DriveStudio version 1.5 before the installation of this Service Pack! ================================================================ *** BEFORE YOU START THE PROGRAM, PLEASE READ THIS CAREFULLY *** ================================================================ This file has been divided into the following sections for easy reference: 1. GETTING HELP 2. INSTALLATION 1. GETTING HELP ---------------- If you want help with DriveStudio it is available from the following sources: - Please use first the context-sensitive on-line help by pressing the F1 key (or read the User Manual). - If you need help with drive parameters press F3 on top of the selected parameter - Secondly please contact the local PC support persons. - Also the 24hour SupportLine is able to help in many cases. Contact them by e-mail address: global.drivessupport@fi.abb.com or by phone +358 50 33 27200. Please provide them with information like operating system version, error message code etc. A local ABB Sales office is also able to fetch information from ABB Library (http://inside.abb.com/Library). 2. INSTALLATION ---------------- DO NOT uninstall DriveStudio version 1.5 before the installation of this Service Pack! Close all other programs before installation of this service pack Use always the ControlPanel Add/Remove Programs-Icon to install and uninstall the DriveStudio Start the Installation program DriveStudio_1.6_SP.exe and follow the instructions. After installation, restart PC. Thank you for reading me!