============================================== The installation program of SLDT, ABB Automation Technology Products AB's LON(R) Device Types for LNT 505. ============================================== LON is a registered trademark of Echelon Corporation. About this description ============================================== This document describes the installation program SLDT. Art.no: 1MRK 001 700-9 Version: 1.2-02 Issue date: 03-04 Author's address: ABB Automation Technology Products AB Substation Automation S-721 59 Västerås, Sweden Tel: +46 21 34 20 00 Fax: +46 21 14 69 18 Introduction ============================================== SLDT is intended for installing the device type descriptions of ABB's products with LON interface into the installation and configuration tool LNT 505, which is a PC software developed and delivered by ABB Oy, Substation Automation in Finland. For configuration of the LON interface for ABB's products, LNT 505 is required, i.e. it is not possible to configure these products using any other commercially available tool. All versions of following products are supported by SLDT: RET 521 REC 561 REL 501 REL 511 REL 521 REL 531 REL 551 REL 561 REB 551 REO 517 For RET 521 two different device type descriptions are included to be used depending on if the target RET 521 terminal has optional voltage control function for 8 parallel transformers (VCTR8) installed or not. The VCTR8 option is only available as from RET 521 v2.4. The installation program SLDT consists of the following files: setup.exe A self installing file that completely installs the device types that are selected by the user. readme.txt Description of SLDT software package. System requirements ============================================== Hardware: A PC capable of running LNT 505. Platform: Windows 3.1x, NT, 95, 98 or 2000. Software: LNT 505 version 1.0.1c or later installed. Installation ============================================== The installation program displays a couple of dialogue windows before the actual installation is started. The installation may be aborted at any time by pressing the button 'Cancel'. The installation procedure is as follows: 1. Run the executable file setup.exe. 2. The installation program welcomes you. Read the information and press button 'Next'. 3. Select the destination directory, i.e. the top directory where the LNT 505 is installed. Use the default directory or browse to the correct directory, then press button 'Next'. 4. Select components, i.e. device types, to install by checking the corresponding check boxes, then press button 'Next'. 5. You will get a message that you now are ready to install. Press button 'Next' and the actual installation will start. 6. The installation is completed. Press 'Finish' button. Next time LNT 505 is started the installed device types may be found in the list of device types. Device types that were previously installed are updated. New device types are added to the LNT 505. Customer feedback ============================================== If you find "features" of this installation program or with the installed device types, which more correctly would be described as bugs, please let us know. Any proposals for improvements are welcomed as well. Legal notice ============================================== We reserve all rights to this document, even in the event that a patent is issued and a different commercial proprietary right is registered. Improper use, in particular reproduction and dissemination to third parties, is not permitted. This document has been carefully checked. If the user nevertheless detects any errors, he is asked to notify us as soon as possible. (C) ABB Automation Technology Products AB 2003